OM13093 schematic

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

OM13093 schematic

2,127 Views
amit1234
NXP Employee
NXP Employee

Hi,

  Does any body have schematic of OM13093?

I just need to confirm I2C pins on this board extension connector.

Thanks.

Labels (1)
0 Kudos
Reply
2 Replies

1,682 Views
Carlos_Mendoza
NXP Employee
NXP Employee

Hi Amit,

Here is the link to the LPCXpresso board LPC11C24 rev B:

http://www.nxp.com/assets/downloads/data/en/schematics/LPCXpressoLPC11C24revB.pdf 

Hope it helps!

Best Regards,
Carlos Mendoza
Technical Support Engineer

Update:

The schematics seem to be for OM13012, will update the thread once I have the one for OM13093.

http://www.nxp.com/assets/downloads/data/en/schematics/LPCXpresso11C24-with-CMSIS-DAP-SCH.pdf 

0 Kudos
Reply

1,682 Views
brendonslade
NXP TechSupport
NXP TechSupport

The schematic should have been posted under the downloads tab for the board - we have corrected this omission now. Please get the schematic here:

http://www.nxp.com/demoboard/OM13093 ... look under the Downloads tab.

0 Kudos
Reply