Om13085 code not executing/starting after Reset

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Om13085 code not executing/starting after Reset

1,319 次查看
ronwal
Contributor III

I´m using the the OM13085 and somehow the code is only executing when connected to the IDE/debugger and right after the firmware have been flashed.

If I reset the board or switch it off and on the code is not executing...

My project is based on the uIP/webserver samples.

Any idea?

Thanks

br Ron

标签 (1)
0 项奖励
回复
1 回复

1,237 次查看
brendonslade
NXP TechSupport
NXP TechSupport

Hi Ron,

I think you also posted this question as response to a previous thread:

https://community.nxp.com/thread/435247?sr=stream

Since I answered that one, I am marking this thread as assumed answered too.

Regards,

Brendon

0 项奖励
回复