Old 2012 Header Files for LPC812

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Old 2012 Header Files for LPC812

Jump to solution
2,203 Views
james_eck
Contributor I

A few years ago, I wrote the attached micro-controller code based on the sample code available at that time. I have since deleted most of the work space and moved onto a new computer, but I am now trying to make some modifications to the code and without the header files I used back then, I can't build the project. Where can I obtain these header files?

#include "lpc8xx_spi.h"
#include "lpc8xx_mrt.h"
#include "lpc8xx_clkconfig.h"
#include "lpc8xx_wdt.h"

Thanks!

Labels (3)
0 Kudos
Reply
1 Solution
2,089 Views
fjrg76
Contributor IV

Maybe here you find what you're looking for:

LPCOpen Software for LPC8XX|NXP 

View solution in original post

0 Kudos
Reply
2 Replies
2,090 Views
fjrg76
Contributor IV

Maybe here you find what you're looking for:

LPCOpen Software for LPC8XX|NXP 

0 Kudos
Reply
2,089 Views
jeremyzhou
NXP Employee
NXP Employee

Hi  James Eck ,

Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
To provide the fastest possible support, please download the code bundles via these below links.
[‎10/‎8/‎2018 9:41 AM]  Kerry Zhou:  
https://www.nxp.com/downloads/en/software/LPC812_Example_Code_Bundle_Keil_IAR_r1.0.00.zip
https://www.nxp.com/downloads/en/software/LPC812_Example_Code_Bundle_LPCXpresso_r1.00.00.zip
Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply