Old 2012 Header Files for LPC812

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Old 2012 Header Files for LPC812

跳至解决方案
2,266 次查看
james_eck
Contributor I

A few years ago, I wrote the attached micro-controller code based on the sample code available at that time. I have since deleted most of the work space and moved onto a new computer, but I am now trying to make some modifications to the code and without the header files I used back then, I can't build the project. Where can I obtain these header files?

#include "lpc8xx_spi.h"
#include "lpc8xx_mrt.h"
#include "lpc8xx_clkconfig.h"
#include "lpc8xx_wdt.h"

Thanks!

标签 (3)
0 项奖励
回复
1 解答
2,152 次查看
fjrg76
Contributor IV

Maybe here you find what you're looking for:

LPCOpen Software for LPC8XX|NXP 

在原帖中查看解决方案

0 项奖励
回复
2 回复数
2,153 次查看
fjrg76
Contributor IV

Maybe here you find what you're looking for:

LPCOpen Software for LPC8XX|NXP 

0 项奖励
回复
2,152 次查看
jeremyzhou
NXP Employee
NXP Employee

Hi  James Eck ,

Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
To provide the fastest possible support, please download the code bundles via these below links.
[‎10/‎8/‎2018 9:41 AM]  Kerry Zhou:  
https://www.nxp.com/downloads/en/software/LPC812_Example_Code_Bundle_Keil_IAR_r1.0.00.zip
https://www.nxp.com/downloads/en/software/LPC812_Example_Code_Bundle_LPCXpresso_r1.00.00.zip
Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复