Old 2012 Header Files for LPC812

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Old 2012 Header Files for LPC812

ソリューションへジャンプ
2,259件の閲覧回数
james_eck
Contributor I

A few years ago, I wrote the attached micro-controller code based on the sample code available at that time. I have since deleted most of the work space and moved onto a new computer, but I am now trying to make some modifications to the code and without the header files I used back then, I can't build the project. Where can I obtain these header files?

#include "lpc8xx_spi.h"
#include "lpc8xx_mrt.h"
#include "lpc8xx_clkconfig.h"
#include "lpc8xx_wdt.h"

Thanks!

ラベル(3)
0 件の賞賛
返信
1 解決策
2,145件の閲覧回数
fjrg76
Contributor IV

Maybe here you find what you're looking for:

LPCOpen Software for LPC8XX|NXP 

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,146件の閲覧回数
fjrg76
Contributor IV

Maybe here you find what you're looking for:

LPCOpen Software for LPC8XX|NXP 

0 件の賞賛
返信
2,145件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi  James Eck ,

Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
To provide the fastest possible support, please download the code bundles via these below links.
[‎10/‎8/‎2018 9:41 AM]  Kerry Zhou:  
https://www.nxp.com/downloads/en/software/LPC812_Example_Code_Bundle_Keil_IAR_r1.0.00.zip
https://www.nxp.com/downloads/en/software/LPC812_Example_Code_Bundle_LPCXpresso_r1.00.00.zip
Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信