OTG and host clock not available

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

OTG and host clock not available

2,257 Views
bamdadslr
Contributor II

Hi,

I am using the MCUXpresso IDE to program a LPC4088 controller. In part of my code I want to initialize the USB host and trying to enable the USB host, OTG clock and AHB master clock. So, I use this instruction

LPC_USB->OTGClkCtrl = 0x00000019.

After that, when I check LPC_USB->OTGClkSt, its binary value is 10000, which shows the device host clock and OTG clock are not available! Can you please help me to find what is wrong?

0 Kudos
Reply
3 Replies

2,225 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

I think that you have to enable the USB gated clock before you write the LPC_USB->OTGClkCtrl = 0x00000019.

You can enable the USB gated clock with the line:

SYSCON->PCONP|=1<<31;

Pls refer to section 3.3.2.2 Power Control for Peripherals registers in UM10562.pdf

If you still can not, i suppose you have to enable the 48MHz USB clock

xiangjun_rong_0-1656998883339.png

 

Hope it can help you

BR

XiangJun Rong

 

0 Kudos
Reply

2,219 Views
bamdadslr
Contributor II

Hi,

Thank you for your response. I actually had "LPC_SC->PCONP |= 0x80000000;" before using "LPC_USB->OTGClkCtrl = 0x00000019;" in my code (PCONP[31] is 0x1 which confirms the USB gate is turned on).

The problem is that when I do "LPC_USB->OTGClkCtrl = 0x00000019", LPC_USB->OTGClkSt is not equal to 0x00000019, which I cannot understand why!

0 Kudos
Reply

2,209 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

Pls try to set the USBDIV with a non-zero value, you'd better get 48MHz USB clock by configuring the register including the USBDIV bits and USBSEL bits.

This is the procedure:

1)LPC_SC->PCONP |= 0x80000000

2)LPC_SC->USBCLKSEL=0x01|xx;

3)LPC_USB->OTGClkCtrl = 0x00000019;

4)checking the LPC_USB->OTGClkSt register

Hope it can help you

BR

XiangJun Rong

 

 

xiangjun_rong_0-1657075233785.png

 

0 Kudos
Reply