OM40006 debug probe not detect by keil

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

OM40006 debug probe not detect by keil

734 次查看
pavithran
Contributor I

I started to use lpc54018 IOT module with base board(OM40006). Tried to connect j8(OM40007) with pc. Board powerup properly but not detected by any port. Then baseboard J7 connector connected with pc. Base board(OM40006) detected by PC as LPC USB device but CMSIS debugger not detected by KEIL software. What type of debugger have to select in keil to download program in to LPC 54018.

 

#lpc54018jet180e  #OM40006  #OM40007

0 项奖励
回复
1 回复

721 次查看
Alexis_A
NXP TechSupport
NXP TechSupport

Hello @pavithran,

This will depend on the firmware that the onboard debugger has, it could be either segger or CMSIS. I will suggest following the instructions in the reference manual of the OM40006 Board, section 3.2.2 Installation steps for use with 3rd party tools (e.g. Keil and IAR). This will help you update the onboard firmware.

Best Regards,

Alexis Andalon

0 项奖励
回复