OM13092: USB1 HS device

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

OM13092: USB1 HS device

1,213 次查看
belmontbob59
Contributor IV

The specs read in section 39.3:

pastedImage_1.png

However the board uses a 12Mhz crystal oscillator:

pastedImage_2.png

Shouldn't the XTAL be 48Mhz instead ? So how is this possible that the USB1 example still run ? what  am  I missing ?

标签 (1)
0 项奖励
回复
1 回复

1,102 次查看
jeremyzhou
NXP Employee
NXP Employee

Hi bob belmont,

Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
I think you misunderstand this statement, it means that developer should beware of configuring a 48 MHz (USB clock), which is not equal to selecting 48 MHz external crystal oscillator.
Hope this is clear.
By the way, I'd like to suggest you build the clock via the MCUXpresso config tool.
Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复