OM13092: USB1 HS device

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

OM13092: USB1 HS device

1,206件の閲覧回数
belmontbob59
Contributor IV

The specs read in section 39.3:

pastedImage_1.png

However the board uses a 12Mhz crystal oscillator:

pastedImage_2.png

Shouldn't the XTAL be 48Mhz instead ? So how is this possible that the USB1 example still run ? what  am  I missing ?

ラベル(1)
0 件の賞賛
返信
1 返信

1,095件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi bob belmont,

Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
I think you misunderstand this statement, it means that developer should beware of configuring a 48 MHz (USB clock), which is not equal to selecting 48 MHz external crystal oscillator.
Hope this is clear.
By the way, I'd like to suggest you build the clock via the MCUXpresso config tool.
Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信