OM13089 strange Power measurement

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

OM13089 strange Power measurement

1,024 Views
Catosh
Contributor IV

I want to measure the power consumption of the MCU on the OM13089 board;
according to the instructions of AN11799 I can probe the current on JP4; the issue that even in reset I am measuring 68mA.
Then from that current level I can see the normal variation on the consumption due to different power level modes. 

Did someone else had this issue?

Any hint would be very appreciated.

B.R.

L

0 Kudos
Reply
1 Reply

909 Views
jeremyzhou
NXP Employee
NXP Employee

Hi Catosh ,

Thank you for your interest in NXP Semiconductor products and 
for the opportunity to serve you. I've done some testing and the AN11799 works well, I'd like to exemplify the testing results.
WeChat Image_20170621103619.jpg
            Fig 1 Normal working mode
WeChat Image_20170621103850.jpg
                              Fig 2 Sleep mode
WeChat Image_20170621103931.jpg
                             Fig 3 Deep sleep mode
WeChat Image_20170621103952.jpg
                                      Fig 4 Deep power mode
Hope it helps.

Have a great day,
TIC

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply