OM13088 V3 Schematic

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

OM13088 V3 Schematic

3,849 Views
yamaoka
Contributor I

Hi,

We've gotten the OM13088 V3 board that is equipped with LPC4367JET256 and want to know how the LPC4367 and the peripherals are configured on the board in order to reflect it into our new product design using LPC4367. Could you let us know where the schematic diagram of it is, or send it to me directly?

Thanks in advance.
Regards,

0 Kudos
Reply
7 Replies

3,834 Views
yamaoka
Contributor I

Hi ZhangJennie,

Thanks for the reply. We already knew those materials existing, however the CPU drawn in the schematic is LPC4322JET100, not LPC4322JET100 that the board we've gotten is equipped with. Could you please show us the schematic that exactly matches the boad?

Thanks.
Regards,

0 Kudos
Reply

3,837 Views
ZhangJennie
NXP TechSupport
NXP TechSupport
0 Kudos
Reply

3,831 Views
yamaoka
Contributor I

Hi ZhangJennie,

Thanks for the reply. I already knew those materials existing, however the CPU drawn in the schematic is LPC4322JET100, not LPC4367JET256 that the board we've gotten is equipped with. Could you please show us the schematic that exactly matches the boad?

Thanks.
Regards,

0 Kudos
Reply

3,822 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

By checking, we only have schematic for LPC4367JET100.

0 Kudos
Reply

3,808 Views
yamaoka
Contributor I

Ok. We interpretted that you don't have a will to open the schematic for the OM13088 V3 board, the version that that is equipped with LPC4367JET256 (we think it can't be non-existent as the board actually exists and is widely distributrd). Thanks anyway for the reply.

0 Kudos
Reply

3,801 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

The MCU Equipped on the board is LPC4367JET100. 

LPC4322 on board is for debug module.

anyway, we don't have the same schematic reference for LPC4367JET256

0 Kudos
Reply

3,798 Views
yamaoka
Contributor I

Ok.  Thanks.

0 Kudos
Reply