OM13077 Target SWD Debug Port - ISP Pin missing

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

OM13077 Target SWD Debug Port - ISP Pin missing

1,745件の閲覧回数
simonwyss
Contributor III

On the OM13077 Development kit, the ISP Pin on the SWD Debug Port is missing. The SWD Header has no pin on position 7!!!

Found this issue while trying to debug / flash a LPC54120 which wasn't responding.
I tried the solutions from the FAQ but no one was working. Then I checked the ISP connection to my board and noticed, that the ISP pin was never pulled low.

I had to connect the ISP (pin 7) manually to my target board.

Thank you NXP, I had some fun debugging, why my target doesn't want to respond. (There was no single note for this issue)

FAQ for target not responding and Debug
Regaining debug access to target MCU 
ISP Reset over debug 

Design Considerations for Debug 

pastedImage_2.png

pastedImage_3.png

ラベル(1)
0 件の賞賛
返信
1 返信

1,573件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi Simon Wyss,

Thank you for your interest in NXP Semiconductor products and 
for the opportunity to serve you.
Getting Jumper JP1 opened, then try again.
Have a great day,

TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信