OLED controller?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

OLED controller?

1,647 次查看
markcianchetti
Contributor I

For the LPC4088 microcontroller, can the LCD controller be used for an OLED?  I see only TFT/STN in the user manual...

标记 (1)
0 项奖励
回复
2 回复数

1,550 次查看
lamose2
Contributor I

Yes it can be, but first better to know exactly what is oled couse in this situation oled structure is not good for that solution

0 项奖励
回复

1,550 次查看
soledad
NXP Employee
NXP Employee

Hi,

 

The controller supports the following types of LCD panel:

  • Active matrix TFT panels with up to 24-bit bus interface.
  • Single-panel monochrome STN panels (4-bit and 8-bit bus interface).
  • Dual-panel monochrome STN panels (4-bit and 8-bit bus interface per panel).
  • Single-panel color STN panels, 8-bit bus interface.
  • Dual-panel color STN panels, 8-bit bus interface per panel.

 

However, you can connect an oled only if the oled has de same type of pins: RGB + HSYNC + VSYNC


Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复