Our customer want to use LPC804 to emulate I2C EEPROM.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Our customer want to use LPC804 to emulate I2C EEPROM.

1,259 次查看
li-chinwang
Contributor II

Our customer want to use LPC804 to emulate I2C EEPROM. 

I saw the example code from NXP. 

After I open it, it is for Keil IDE.

My customer use MCUxpresso.

Does NXP has it for MCUxpresso version?

if yes, please offer it to me.

http://www.nxpic.org/document/detail/index/id-14931

pastedImage_2.png

标签 (2)
0 项奖励
回复
1 回复

1,026 次查看
victorjimenez
NXP TechSupport
NXP TechSupport

Hello Li-Chin Wang,

Please noticed that the link that you attached is not official from NXP. In the following link you can download the official application note along with the code: 

In the .zip you will find a folder named Source_Code the code that is located in this folder can be used with MCUXpresso. Also, the LPC804 now has an SDK you can download it from the following page: 

In the SDK you will find examples of the I2C protocol among any others. 

Hope it helps!

Victor.

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复