Not able to copy more than 8 kB data at a time into Flash bank LPC1833

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Not able to copy more than 8 kB data at a time into Flash bank LPC1833

跳至解决方案
1,678 次查看
ketulpatel
Contributor II

Hello,

We are using LPC1833 in our project. In which we are flashing an image of 87 kB size.

But not able to use more than 8 kB of Flash Buffer size to flash the image.

How we can use more than 8 kB of buffer for the same?

Thanks,
Ketul

标记 (1)
0 项奖励
回复
1 解答
1,623 次查看
Omar_Anguiano
NXP TechSupport
NXP TechSupport

Hello

Hope you are well.
Unfortunately, the supported values of bytes to be written are the ones listed in the reference manual.

Omar_Anguiano_0-1627685148179.png


I apologize for the inconvenience this may cause you, if you have more questions do not hesitate to ask me.
Best regards,
Omar

在原帖中查看解决方案

2 回复数
1,595 次查看
ketulpatel
Contributor II

Thank You!

0 项奖励
回复
1,624 次查看
Omar_Anguiano
NXP TechSupport
NXP TechSupport

Hello

Hope you are well.
Unfortunately, the supported values of bytes to be written are the ones listed in the reference manual.

Omar_Anguiano_0-1627685148179.png


I apologize for the inconvenience this may cause you, if you have more questions do not hesitate to ask me.
Best regards,
Omar