Not able to copy more than 8 kB data at a time into Flash bank LPC1833

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Not able to copy more than 8 kB data at a time into Flash bank LPC1833

Jump to solution
1,684 Views
ketulpatel
Contributor II

Hello,

We are using LPC1833 in our project. In which we are flashing an image of 87 kB size.

But not able to use more than 8 kB of Flash Buffer size to flash the image.

How we can use more than 8 kB of buffer for the same?

Thanks,
Ketul

Tags (1)
0 Kudos
Reply
1 Solution
1,629 Views
Omar_Anguiano
NXP TechSupport
NXP TechSupport

Hello

Hope you are well.
Unfortunately, the supported values of bytes to be written are the ones listed in the reference manual.

Omar_Anguiano_0-1627685148179.png


I apologize for the inconvenience this may cause you, if you have more questions do not hesitate to ask me.
Best regards,
Omar

View solution in original post

2 Replies
1,601 Views
ketulpatel
Contributor II

Thank You!

0 Kudos
Reply
1,630 Views
Omar_Anguiano
NXP TechSupport
NXP TechSupport

Hello

Hope you are well.
Unfortunately, the supported values of bytes to be written are the ones listed in the reference manual.

Omar_Anguiano_0-1627685148179.png


I apologize for the inconvenience this may cause you, if you have more questions do not hesitate to ask me.
Best regards,
Omar