New update

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
1,691件の閲覧回数
Nadia
Contributor III
Good afternoon, I've been using this programming platform for a while, and they've updated it and I'm a bit lost. I have the MUCXpresso IDE v 11.3.0_522 version, I am using the LPC54616J512 microcontroller, when I go to create a new program with the FREErtos operating system, in the source folder I don't see the FREErtosConfig file to access its configuration. I want to know if it happens to someone else and it is something of the update or is it me, and I would like to know how to do it now with this new update. Thank you very much for your help. Best regards
0 件の賞賛
返信
1 解決策
1,673件の閲覧回数
Omar_Anguiano
NXP TechSupport
NXP TechSupport

Hello

When you create a new project from the wizard, you can find the FreeRTOSConfig.h file in this location: Project->freertos->template->ARM_CM4F.

nxf54944_0-1616189323760.pngnxf54944_0-1616189323760.png

Let me know if this is helpful, if you have more questions do not hesitate to ask me.
Best regards,
Omar

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,674件の閲覧回数
Omar_Anguiano
NXP TechSupport
NXP TechSupport

Hello

When you create a new project from the wizard, you can find the FreeRTOSConfig.h file in this location: Project->freertos->template->ARM_CM4F.

nxf54944_0-1616189323760.pngnxf54944_0-1616189323760.png

Let me know if this is helpful, if you have more questions do not hesitate to ask me.
Best regards,
Omar

0 件の賞賛
返信