New LPC Microcontrollers Optimized for System Design Flexibility

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

New LPC Microcontrollers Optimized for System Design Flexibility

2,249 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by NXP_Support on Thu Dec 05 03:12:01 MST 2013
NXP LPC11E37H and LPC11U37H feature new I/O Handler functionality to simplify system design changes. More information at:

http://www.nxp.com/news/press-releases/2013/12/new-lpc-microcontrollers-optimized-for-system-design-...


标签 (1)
0 项奖励
回复
4 回复数

2,229 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by MarcVonWindscooting on Sun Jan 05 09:00:26 MST 2014

Quote: starblue
What I don't like so much:

From UM10462:
"23.5 Register description
The I/O Handler has no user-programmable register interface."



I don't like, neither. And I'm not going to use that, definitely!
It sounds like a cool piece of programmable logic and 'they' (NXP) don't allow us free access. :quest:

Programmers like me, who use open-source develpment tool are completely locked out of programmable logic and that's the sole reason I don't use programmable logic any more since years. I'm sad about that.
I liked the 'open' nature of the LPC's (open bootloader protocol => open software) since my first contact of LPC2106 280 million seconds ago and that's why I stick to LPCs. I started using LPC800 and LPC1100 only a few months ago and LPC1100 already made it into the companies products.

However, I'm known not to fall for an easy temptation at the cost a freedom. All the red lights and sirens went on, when I read Chapter 23 of UM10462: that's exactly the kind of temptation that costs freedom.
If we accept that, then there's more to come.
The time of diminishing human rights, privacy and freedom we are living in should stop us from giving up control deliberately and hand it over to some 'proprietary' code/library.

Read! Understand! Verify! Use! Verify again!

Do NOT: simply use and don't understand and don't (be able to) verify - even if so-called professionals tell you, you don't have the time to do things the hard way these days.
It's the same as f**king b**ches instead of engaging in a reliable partnership, just because the former is cheaper and gives you first success rather quickly ;-)
0 项奖励
回复

2,229 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by starblue on Thu Dec 05 06:13:27 MST 2013
What I don't like so much:

From UM10462:
"23.5 Register description
The I/O Handler has no user-programmable register interface."
0 项奖励
回复

2,229 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Pacman on Thu Dec 05 04:07:28 MST 2013
You have I2S on a M0 device. Cool - very cool! :)
-And USB too, I think it's the first time I've seen that.

Soon a lot of people will manufacture low-cost USB audio devices, which outputs a quite good quality audio. This will also make a new market for low-cost digital audio mixers and digital audio effect devices. Good move! :)
0 项奖励
回复

2,229 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by R2D2 on Thu Dec 05 03:38:25 MST 2013
The new I/O Handler peripheral allows designers to easily add significant functionality, such as [color=#f00]serial communications interfaces[/color], at any time in the design cycle. 


Does that mean that it's possible to add CAN ????
0 项奖励
回复