Need of working SPI driver for LPC11A04

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Need of working SPI driver for LPC11A04

1,347 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by RatheeshT on Tue Jan 05 03:27:58 MST 2016
Hi, 

    I tried SPI driver in loop back mode , it is working fine. To communicate with external device, i tried to use SPI in polling and interrupt modes. I cannot find it is working or not.
Please tell me how can i  check ?

Specification -;

SPI frequency - 8MHZ (set by me )
IDE used - LPCXpresso v7.9 2_493  
Platform - windows 7

Thanks in advance

Regards,

Ratheesh T
标签 (1)
0 项奖励
回复
2 回复数

1,334 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by RatheeshT on Tue Jan 05 23:19:54 MST 2016
HI,

First thank you for quick response, i will try on board to board communication.

I am testing SPI with older version v1.03. Is it available SPI V2.03 ( latest version ). Pls give me the exact link for latest version of SPI driver.


Thanks & regards ,
Ratheesh T
0 项奖励
回复

1,334 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by mc on Tue Jan 05 08:56:34 MST 2016
Hi Ratheesh T,
If you have two board you can make LPC on one board as a master and the LPC on another board as a slave. If you do not have two board you can communicate with any SPI-based EEPROM.
0 项奖励
回复