Need MCU advice

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Need MCU advice

2,926件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by bobi-one on Mon Mar 24 05:19:31 MST 2014
Hi Community,
I am stuck at simple conundrum.
I Need low pin count micro-controller
that needs to drive micro sd card and external SPI dac.
the purpose is to be able to read and play 2-3 wave files(16bit 22050) at the same time from the card.
I was using lpc1343 and was able to play one but i wasn't able to play second one without using the whole resource of the controller. So I think I need DMA to make it more robust.
So if you have any suggestion what kind of NXP controller have DMA,  low pin count and etc. please share your  thoughts here.
I will really appreciate any further advice.
Regards,
Boyko
ラベル(1)
0 件の賞賛
返信
5 返答(返信)

2,916件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by LabRat on Tue Mar 25 01:26:30 MST 2014

Quote: bobi-one
Did you design custom board for those...



5


Quote: bobi-one
...did you had any difficulties  doing so?



No.
0 件の賞賛
返信

2,916件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by bobi-one on Tue Mar 25 01:18:12 MST 2014
Did you design custom board for those, and did you had any difficulties  doing so?
Those chip have really power supply pin placement but may need more thinking before doing so.
Regards,
Boyko
0 件の賞賛
返信

2,916件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by LabRat on Mon Mar 24 07:29:24 MST 2014

Quote: bobi-one
Are you familiar with more specific difference between the  three like clock speed and som other limitations?



I'm using LPC1549 in LQFP48 and LQFP64: 256kB Flash, 36kB SRAM, 4kB EEPROM, 72MHz, ROM-CAN and ROM-USB as described in Datasheet / User manual...

http://www.nxp.com/products/microcontrollers/cortex_m3/LPC1549JBD48.html


0 件の賞賛
返信

2,916件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by bobi-one on Mon Mar 24 07:13:11 MST 2014
Thank you for the fast responce.
I am not familiar with this family of products,
So there is 1517 and 1547 and 1549 with a different pinout. Are you familiar with more specific difference between the  three like clock speed and som other limitations?
Regards,
Boyko
0 件の賞賛
返信

2,916件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by LabRat on Mon Mar 24 05:57:30 MST 2014
New LPC15xx in LQFP48?
0 件の賞賛
返信