NXP LPC Arm LCD compatibility

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

NXP LPC Arm LCD compatibility

1,192 Views
jonathansmith
Contributor III

I'm looking at starting some development using the LPC4357-K43WQA development board. It is for a project that needs an LCD screen. LPC ARM devices are what we have the most experience with here, so the development board that uses an LPC4357 and comes with an LCD screen looks like an obvious choice.

I see that it uses a K43WQA screen, but these aren't widely available and I would like to have a choice of screen sizes, and ones that are easier to source.

Is there an alternative screen that will work with the LPC4357? I can't work out what the interface is. If it's a standard interface then I guess I can have a choice of different screen sizes to work with?

Thanks in advance.

Labels (2)
0 Kudos
Reply
0 Replies