NXP LPC Arm LCD compatibility

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

NXP LPC Arm LCD compatibility

1,216件の閲覧回数
jonathansmith
Contributor III

I'm looking at starting some development using the LPC4357-K43WQA development board. It is for a project that needs an LCD screen. LPC ARM devices are what we have the most experience with here, so the development board that uses an LPC4357 and comes with an LCD screen looks like an obvious choice.

I see that it uses a K43WQA screen, but these aren't widely available and I would like to have a choice of screen sizes, and ones that are easier to source.

Is there an alternative screen that will work with the LPC4357? I can't work out what the interface is. If it's a standard interface then I guess I can have a choice of different screen sizes to work with?

Thanks in advance.

ラベル(2)
0 件の賞賛
返信
0 返答(返信)