NFC Reader library - multiple RC663 on one LPC1769

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

NFC Reader library - multiple RC663 on one LPC1769

2,816件の閲覧回数
DenisP
Contributor II

Hi

Is it possible to connect multiple RC663 reader chips to different UARTs in LPC1769 using the Reader Library

Thank you

ラベル(1)
タグ(2)
0 件の賞賛
返信
3 返答(返信)

2,805件の閲覧回数
fangfang
NXP TechSupport
NXP TechSupport

Hello,

The examples of the NFC Reader Library are for SPI communication. So the customer can't use the NFC Library via UART.

Have a nice day.

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-----------------------------------------------------------------------------

 

0 件の賞賛
返信

2,791件の閲覧回数
DenisP
Contributor II

Thank you

But there are parameters in the library

PHHAL_HW_BAL_CONNECTION_RS232

PHHAL_HW_BAL_CONNECTION_SPI

PHHAL_HW_BAL_CONNECTION_I2C

Doesn't this mean that I can use the reader library with RC663 connected via RS232?

0 件の賞賛
返信

2,781件の閲覧回数
fangfang
NXP TechSupport
NXP TechSupport

Hello,

Yes, RC663 can supports RS232.

Please find more information as the link.

URL:https://www.nxp.com/docs/en/data-sheet/CLRC663.pdf.

But the library supports SPI. If the customer needs RS232 and needs to design it themselves.

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-----------------------------------------------------------------------------

0 件の賞賛
返信