NAND Flash with LPC55S16

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

NAND Flash with LPC55S16

2,958件の閲覧回数
nxf64834
NXP Employee
NXP Employee
Hi, Can we interface NAND Flash with LPC55S16? If yes, what is the maximum memory size that can be interfaced? Also, what's the alternate for NAND flash which is compatible with LPC55S16? There is no info available regarding this in datasheet or RM. Thanks in advance!!
0 件の賞賛
返信
3 返答(返信)

2,946件の閲覧回数
Alexis_A
NXP TechSupport
NXP TechSupport

Hello @nxf64834,

The LPC55s16 doesn't have an external memory controller or SPIFI interface so the only memories supported will be the ones using SPI/I2C interface.

Best Regards,
Alexis Andalon

0 件の賞賛
返信

2,931件の閲覧回数
nxf64834
NXP Employee
NXP Employee

Hi Alexis, 

Thanks for the info.

For NOR flash using SPI, is there any maximum memory size limit that can be interfaced with LPC?

As per my understanding, external memory flash address are not mapped to microcontroller so there should be no size limit.

 

0 件の賞賛
返信

2,916件の閲覧回数
Alexis_A
NXP TechSupport
NXP TechSupport

Hello @nxf64834,

That's right, this will depend on the memory and how to commands are implemented.

Best Regards,

Alexis Andalon

0 件の賞賛
返信