FCn_SSEL2 and FCn_SSEL3 are only on FC3 and FC4 in LPC54608.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

FCn_SSEL2 and FCn_SSEL3 are only on FC3 and FC4 in LPC54608.

ソリューションへジャンプ
1,575件の閲覧回数
toipaz
Contributor III

Datasheet says FCn can use a total of four Slave selections,
LPC54608 pin description shows that only FC3 and FC4 have SSEL2 and SSEL3.
Can't I use SSEL2 and SSEL3 for other FC0 to FC2, FC5 to FC9?

 

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
1,566件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi toipaz

Yes, for LPC546xx, only FC3 and FC4 have SSEL2 and SSEL3.

 

Have a nice day,

Jun Zhang

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
1,567件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi toipaz

Yes, for LPC546xx, only FC3 and FC4 have SSEL2 and SSEL3.

 

Have a nice day,

Jun Zhang

0 件の賞賛
返信
1,559件の閲覧回数
toipaz
Contributor III

Thanks for your reply.

I tried to use it after seeing the datasheet that supports up to four, but it is very sad for me.

So, we're trying to expand using GPIO.
0 件の賞賛
返信
1,556件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

toipaz

It declares supporting up to 4. It doesn't mean every FCn can support up to 4.

For LPC546xx, only FC3 and FC4 can support SSEL0-SSEL3.

Hope this clarify the issue.

 

Best Regards

Jun Zhang 

0 件の賞賛
返信