Motion Control by LPC43xx

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Motion Control by LPC43xx

1,256件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by rezaxyz on Mon Apr 20 03:54:54 MST 2015
Hi all,

I'm planning to design an industrial robot which should have a position feedback from multiple axises (minimum of 3) and control them by servo motors, So I have 2 questions:

1. Since LPC microcontrollers have only one QEI, is it possible to decode multiple quadrature encoders by LPC43xx SGPIOs and SCT?

2. Is it possible to generate sophisticated motion pulses to feed servo drivers by SGPIOs and SCT?

Any help appreciated,
Reza
ラベル(1)
0 件の賞賛
返信
1 返信

1,202件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by rezaxyz on Fri Apr 24 08:54:22 MST 2015
Hi,

There is a AN from NXP about interfacing camera to MCU by means of SGPIO, since decoding camera pulses is more complicated than quadrature encoder, It seems the answer of my above question be positive. Nevertheless I'd like to know your opinion.

0 件の賞賛
返信