Need to configure pin P8_1 as GPIO interrupt

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Need to configure pin P8_1 as GPIO interrupt

1,148 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by alston_gama on Fri May 30 01:34:08 MST 2014
Hi ,

I want to configure pin [u]P8.1 FUNC0 => GPIO4[1][/u] as GPIO interrupt.
I have added lpc43xx_gpio.h and lpc43xx_gpio.c files to my project.

and thinking of use below driver routine

/*********************************************************************//**
* @briefEnable GPIO interrupt (just used for P0.0-P0.30, P2.0-P2.13)
* @param[in]portNumPort number to read value, should be: 0 or 2
* @param[in]bitValueValue that contains all bits on GPIO to enable,
* should be in range from 0 to 0xFFFFFFFF.
* @param[in]edgeStatestate of edge, should be:
* - 0: Rising edge
* - 1: Falling edge
* @returnNone
**********************************************************************/
void GPIO_IntCmd(uint8_t portNum, uint32_t bitValue, uint8_t edgeState)
{
...
}

but according to the description given Port number to read value, should be: 0 or 2.

So, does it mean pin P8.1 FUNC0 => GPIO4[1] can not be used as GPIO interrupt pin?!

Note: I am using Embedded Artist LPC4357 dev kit and Embedded Artist LCD disply board ( EA LCD 004 ).
P8_1 is used for touch interrupt.

Thanks, 
Labels (1)
0 Kudos
Reply
1 Reply

1,045 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by embd02161991 on Fri May 30 11:48:17 MST 2014
Hi,

Any GPIO pin can be used as a pin interrupt. Hence, Pin P8_1 can be used as a GPIO interrupt pin.

You can refer to GPIO Pin interrupt function in LPC18xx  and implement a similar one for your application.

Have you checked out the LPCOpen software platform examples? They have  the latest libraries.

Please visit : 
http://www.lpcware.com/content/nxpfile/lpcopen-software-development-platform-lpc43xx-packages

Thanks,

NXP Technical support
0 Kudos
Reply