Migrating from LPC1343 to LPC1347

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Migrating from LPC1343 to LPC1347

ソリューションへジャンプ
3,577件の閲覧回数
Magnetron
Contributor III

Hi, ALL

I'm successfully migrate SW from LPC1343 to LPC1347, except FW upgrade via USB IAP.

This is my SW code that run on LPC1343 and not run on LPC1347:

#define init_msdstate() *((uint32_t *)(0x10000054)) = 0x00000000

.....

/* Disable SYSTICK timer and interrupt before calling into ISP */
SysTick->CTRL &= ~(SysTick_CTRL_ENABLE_Msk | SysTick_CTRL_TICKINT_Msk);

/* Initialize Storage state machine */
init_msdstate();

/*
* Set stack pointer to ROM value (reset default) This must be the last
* piece of code executed before calling ISP, because most C expressions
* and function returns will fail after the stack pointer is changed.
*/
__set_MSP( * ( (uint32_t *) 0x1FFF0000 ) );

/*
* Invoke ISP. We call "iap_entry" to invoke
* ISP because the ISP entry is done through the same
* command interface as IAP.
*/
flash_LPC13XX_IAP_ReInvokeISP();

/* Code will never return! */

......

Because I use RAM2 for USB drivers, I changed  #define init_msdstate() to:

#define init_msdstate() *((uint32_t *)(0x20004054)) = 0x00000000

BUT, it still doesn't works.

Whats wrong?

0 件の賞賛
返信
1 解決策
3,305件の閲覧回数
Magnetron
Contributor III

O'key. I found the problem.

I don't know why, but if I change this line

__set_MSP( * ( (uint32_t *) 0x1FFF0000 ) );

to this one

__set_MSP( * ( (uint32_t *) 0x00000000 ) );

and USB bootloader running!

 

BUT, if I apply optimization by size, the USB bootloader not running.

I think it is because a BUG in compiler in LPCXpresso 8.2.2 that I use.

I find WORKAROUND for this BUG, I use volatile value assigned to zero, like this:

volatile uint32_t topOfStack = 0;

__set_MSP( * ( (uint32_t *) topOfStack) );

I prefer to use _vStackTop value defined in linker script:

.....

    PROVIDE(_vStackTop = DEFINED(__user_stack_top) ? __user_stack_top : __top_Ram);

.....

So finally, this is my ReInvokeISP function that run on LPC1347 with ANY optimization:

.....

#define init_msdstate() *((uint32_t *)(0x10000054)) = 0x00000000

extern void _vStackTop(void);

.......

void ReInvokeISP()
{

/* Disable IRQ specific interrupts */

/* DON'T use __disable_irq()       */
NVIC_DisableIRQ(PIN_INT0_IRQn);
NVIC_DisableIRQ(PIN_INT1_IRQn);
NVIC_DisableIRQ(PIN_INT2_IRQn);
NVIC_DisableIRQ(PIN_INT3_IRQn);
NVIC_DisableIRQ(PIN_INT4_IRQn);
NVIC_DisableIRQ(PIN_INT5_IRQn);
NVIC_DisableIRQ(PIN_INT6_IRQn);
NVIC_DisableIRQ(PIN_INT7_IRQn);
NVIC_DisableIRQ(GINT0_IRQn);
NVIC_DisableIRQ(GINT1_IRQn);
NVIC_DisableIRQ(RIT_IRQn);
NVIC_DisableIRQ(SSP1_IRQn);
NVIC_DisableIRQ(I2C_IRQn);
NVIC_DisableIRQ(CT16B0_IRQn);
NVIC_DisableIRQ(CT16B1_IRQn);
NVIC_DisableIRQ(CT32B0_IRQn);
NVIC_DisableIRQ(CT32B1_IRQn);
NVIC_DisableIRQ(SSP0_IRQn);
NVIC_DisableIRQ(USART_IRQn);
NVIC_DisableIRQ(USB_IRQ_IRQn);
NVIC_DisableIRQ(USB_FIQ_IRQn);
NVIC_DisableIRQ(ADC_IRQn);
NVIC_DisableIRQ(BOD_IRQn);
NVIC_DisableIRQ(FMC_IRQn);
NVIC_DisableIRQ(USBWAKEUP_IRQn);

/*

 * Don't use NVIC_DisableIRQ(WDT_IRQn); 

 * because you need WDT for MCU reset after firmware.bin replacement

 */

/* Disable SYSTICK timer and interrupt before calling into ISP */
SysTick->CTRL &= ~(SysTick_CTRL_ENABLE_Msk | SysTick_CTRL_TICKINT_Msk);

/* Initialize Storage state machine */
init_msdstate();

/*
* Reset main stack pointer. This must be the last piece of code
* executed before calling ISP, because most C expressions and
* function returns will fail after the stack pointer is changed.
*/
__set_MSP((uint32_t) &_vStackTop);

/*
* Invoke ISP. We call "iap_entry" to invoke
* ISP because the ISP entry is done through the same
* command interface as IAP.
*/
flash_LPC13XX_IAP_ReInvokeISP();

/* Code will never return! */
}

I attached useful drivers that can help you.

Have a good day!

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
3,306件の閲覧回数
Magnetron
Contributor III

O'key. I found the problem.

I don't know why, but if I change this line

__set_MSP( * ( (uint32_t *) 0x1FFF0000 ) );

to this one

__set_MSP( * ( (uint32_t *) 0x00000000 ) );

and USB bootloader running!

 

BUT, if I apply optimization by size, the USB bootloader not running.

I think it is because a BUG in compiler in LPCXpresso 8.2.2 that I use.

I find WORKAROUND for this BUG, I use volatile value assigned to zero, like this:

volatile uint32_t topOfStack = 0;

__set_MSP( * ( (uint32_t *) topOfStack) );

I prefer to use _vStackTop value defined in linker script:

.....

    PROVIDE(_vStackTop = DEFINED(__user_stack_top) ? __user_stack_top : __top_Ram);

.....

So finally, this is my ReInvokeISP function that run on LPC1347 with ANY optimization:

.....

#define init_msdstate() *((uint32_t *)(0x10000054)) = 0x00000000

extern void _vStackTop(void);

.......

void ReInvokeISP()
{

/* Disable IRQ specific interrupts */

/* DON'T use __disable_irq()       */
NVIC_DisableIRQ(PIN_INT0_IRQn);
NVIC_DisableIRQ(PIN_INT1_IRQn);
NVIC_DisableIRQ(PIN_INT2_IRQn);
NVIC_DisableIRQ(PIN_INT3_IRQn);
NVIC_DisableIRQ(PIN_INT4_IRQn);
NVIC_DisableIRQ(PIN_INT5_IRQn);
NVIC_DisableIRQ(PIN_INT6_IRQn);
NVIC_DisableIRQ(PIN_INT7_IRQn);
NVIC_DisableIRQ(GINT0_IRQn);
NVIC_DisableIRQ(GINT1_IRQn);
NVIC_DisableIRQ(RIT_IRQn);
NVIC_DisableIRQ(SSP1_IRQn);
NVIC_DisableIRQ(I2C_IRQn);
NVIC_DisableIRQ(CT16B0_IRQn);
NVIC_DisableIRQ(CT16B1_IRQn);
NVIC_DisableIRQ(CT32B0_IRQn);
NVIC_DisableIRQ(CT32B1_IRQn);
NVIC_DisableIRQ(SSP0_IRQn);
NVIC_DisableIRQ(USART_IRQn);
NVIC_DisableIRQ(USB_IRQ_IRQn);
NVIC_DisableIRQ(USB_FIQ_IRQn);
NVIC_DisableIRQ(ADC_IRQn);
NVIC_DisableIRQ(BOD_IRQn);
NVIC_DisableIRQ(FMC_IRQn);
NVIC_DisableIRQ(USBWAKEUP_IRQn);

/*

 * Don't use NVIC_DisableIRQ(WDT_IRQn); 

 * because you need WDT for MCU reset after firmware.bin replacement

 */

/* Disable SYSTICK timer and interrupt before calling into ISP */
SysTick->CTRL &= ~(SysTick_CTRL_ENABLE_Msk | SysTick_CTRL_TICKINT_Msk);

/* Initialize Storage state machine */
init_msdstate();

/*
* Reset main stack pointer. This must be the last piece of code
* executed before calling ISP, because most C expressions and
* function returns will fail after the stack pointer is changed.
*/
__set_MSP((uint32_t) &_vStackTop);

/*
* Invoke ISP. We call "iap_entry" to invoke
* ISP because the ISP entry is done through the same
* command interface as IAP.
*/
flash_LPC13XX_IAP_ReInvokeISP();

/* Code will never return! */
}

I attached useful drivers that can help you.

Have a good day!

0 件の賞賛
返信
3,305件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi Denys Yurchenko ,

Thank you for your interest in NXP Semiconductor products and 
for the opportunity to serve you.
According to your states, you suspect that the macro #define init_msdstate()

#define init_msdstate() *((uint32_t *)(0x20004054)) = 0x00000000 cause this issue, and I'd like to share some suggestion about this issue.

1. Whether you had tried assign the storage state machine in RAM1.

2. Whether you can assure USBSRAM bit has became 1.

Have a great day,
TIC

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
3,305件の閲覧回数
Magnetron
Contributor III

1. Yes, I tried use RAM1 instead RAM2. The same result, not working.

2. What is USBSRAM?

0 件の賞賛
返信
3,306件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi Denys Yurchenko ,

Thanks for your reply.

I was wondering if you can introduce the demo code in details, and it will help me to figure out the root cause of issue.

Regrading to the USBSRAM bit, it is used to enable or disable the USB SRAM block which has been indicated in the Table 19 in reference manual.

pastedImage_1.png

Have a great day,
TIC

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信