Message RAM in CAN controller on LPC54618

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Message RAM in CAN controller on LPC54618

2,879 次查看
carstenhoffmann
Contributor I

I am using the LPCXpresso54618 demo board with CAN FD kit.

Do I have to instruct the linker not to use the RAM area I dedicated to the CAN controller?

How is this done?

I cannot find any hint in the provided CAN example software.

In the demo the message RAM starts at 0x2001000.

The memory configuration tells the linker to use the whole 160kB RAM area.

Is this correct?

Thanks for your help,

Carsten

标签 (1)
0 项奖励
回复
4 回复数

2,591 次查看
carstengroen
Senior Contributor II

Carsten,

please also have a look at Norbert and my findings here: https://community.nxp.com/thread/464785 

(sorry, can't help you if you are using MCUExpresso, using Keil on my end)

0 项奖励
回复

2,591 次查看
carstenhoffmann
Contributor I

Thanks Carsten,

I noticed the other thread. Still not solved...

Could there be a correlation between both subjects?

Do you instruct your linker not to use the CAN message RAM?

0 项奖励
回复

2,591 次查看
carstengroen
Senior Contributor II

Hi Carsten,

I use a scatter file for the linker which basically tells the linker to keep away from the memory I have allocated (using the "at" attribute) for the CAN ROM API.

I'm sorry, I don't know the details of the MCUExpresso!

0 项奖励
回复

2,591 次查看
carstenhoffmann
Contributor I

Thank you Carsten,

since this is a beginner's question maybe somebody else can help doing this with MCUXpresso.

0 项奖励
回复