Message RAM in CAN controller on LPC54618

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Message RAM in CAN controller on LPC54618

2,874件の閲覧回数
carstenhoffmann
Contributor I

I am using the LPCXpresso54618 demo board with CAN FD kit.

Do I have to instruct the linker not to use the RAM area I dedicated to the CAN controller?

How is this done?

I cannot find any hint in the provided CAN example software.

In the demo the message RAM starts at 0x2001000.

The memory configuration tells the linker to use the whole 160kB RAM area.

Is this correct?

Thanks for your help,

Carsten

ラベル(1)
0 件の賞賛
返信
4 返答(返信)

2,586件の閲覧回数
carstengroen
Senior Contributor II

Carsten,

please also have a look at Norbert and my findings here: https://community.nxp.com/thread/464785 

(sorry, can't help you if you are using MCUExpresso, using Keil on my end)

0 件の賞賛
返信

2,586件の閲覧回数
carstenhoffmann
Contributor I

Thanks Carsten,

I noticed the other thread. Still not solved...

Could there be a correlation between both subjects?

Do you instruct your linker not to use the CAN message RAM?

0 件の賞賛
返信

2,586件の閲覧回数
carstengroen
Senior Contributor II

Hi Carsten,

I use a scatter file for the linker which basically tells the linker to keep away from the memory I have allocated (using the "at" attribute) for the CAN ROM API.

I'm sorry, I don't know the details of the MCUExpresso!

0 件の賞賛
返信

2,586件の閲覧回数
carstenhoffmann
Contributor I

Thank you Carsten,

since this is a beginner's question maybe somebody else can help doing this with MCUXpresso.

0 件の賞賛
返信