Memory resources used for boot loader for LPC54606

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Memory resources used for boot loader for LPC54606

1,435件の閲覧回数
Jetcitycowboy
NXP Employee
NXP Employee

I also have a separate but related question around the internal flash programming. Is the only way to program/erase the internal flash, from the user application code or the IAR flash writer’s monitor code, by calling the IAP (boot rom) flash programming APIs? If so, can you please clarify on the amount of SRAM0 these boot ROM/IAP can use? 41.3.8.2 is troubling. If the internal boot rom/IAP calls require access to the SRAM0 (or other memory/shared resources) then Microsoft needs to have a list of all such usages, for their secondary boot loader.   If their application needs to call the IAP APIs then they would need to budget resources accordingly.  Thank you.

0 件の賞賛
返信
1 返信

1,327件の閲覧回数
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi ,

Please check my feedback at the thread below:

https://community.nxp.com/thread/449736 

best regards,

Hui

0 件の賞賛
返信