Making USB-1 work on LPC1837

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Making USB-1 work on LPC1837

1,257件の閲覧回数
gvk51
Contributor III

I have seen couple of folks asking this question, and even this was a question me until I debugged the issue. I have chosen usbd_rom_hid_keyboard example for explaining. This example uses USB0 for demonstrating HID_Keybaord functionality.

 

To make the same example to work with USB-1, we need the following changes.

1) comment "#define USE_USB0" in app_usbd_cfg.h file

/* #define USE_USB0 */

2) Enable clock for USB-1, I have defined the following function

/**

* @brief enables power for USB1

* @return Nothing

*/

void pwrEnable_USB1(){

  /* Setup GPIOs for USB demos */

  Chip_SCU_PinMux(0x2, 6, (MD_PUP | MD_EZI), FUNC4); /* P2_6 USB1_PWR_EN, USB1 VBus function */

  Chip_SCU_PinMux(0x2, 5, (MD_PLN | MD_EZI | MD_ZI), FUNC2); /* P2_5 USB1_VBUS, MUST CONFIGURE THIS SIGNAL FOR USB1 NORMAL OPERATION */

  Chip_GPIO_WriteDirBit(LPC_GPIO_PORT, 5, 6, true); /* GPIO5[6] = USB1_PWR_EN */

  Chip_GPIO_WritePortBit(LPC_GPIO_PORT, 5, 6, true); /* GPIO5[6] output high */

}

 

Call the above function in hid_main

Board_Init();

pwrEnable_USB1();

/* enable clocks and pinmux */

USB_init_pin_clk();

ラベル(2)
タグ(2)
0 件の賞賛
返信
0 返答(返信)