MMC Interface

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MMC Interface

1,452件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by toad on Fri May 02 12:52:25 MST 2014
The JEDEC standard for eMMC 4.4 introduces the dual data rate. Does the NXP part support this dual data rate? I don't see any mention of it although the user manual says the SD/MMC interface supports MMC version 4.4. Thanks.
ラベル(1)
0 件の賞賛
返信
1 返信

1,415件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by xianghuiwang on Fri May 16 12:15:21 MST 2014
Hi, toad,

We have not validated the dual data rate function. The understanding is the protocol is probably supported - however, the eMMC 4.4 dual data rate is specified at 1.8V which this part does not support.

Thanks!
0 件の賞賛
返信