MIDI USB host examples

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MIDI USB host examples

3,038件の閲覧回数
jking1
Contributor II

Hi

Has anyone got any  example code or project to implement a USB MIDI host on, for example, the LPC54628?

In the SDK there are example projects for HID, MSD, CDC etc. but nothing for  MIDI. 

I'm aware of  nxpUSBlib from around 2016, but I'm looking for something that is based on the code structure of the current SDK host examples so that I can efficiently drop in support for MIDI along side other device classes.

Thanks

 

0 件の賞賛
返信
3 返答(返信)

3,025件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi jking1 

Unfortunately our SDK for LPC54xxx doesn't integrate USB MIDI  samples.

Jun Zhang

0 件の賞賛
返信

3,022件の閲覧回数
jking1
Contributor II

Hi

I'm well aware that the LPC54xxx does not have any midi host examples.  I'm hoping that the wider community might be able to provide some insight or assistance.

Is there a reason that midi is not covered in the current SDKs? 

Regards

0 件の賞賛
返信

3,017件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

What demo code is included in SDK is a market decision.

As I know lpcopen for LPC176x includes USB MIDI host code. You can take a look at MIDIClassHost.c/h file. However SDK doesn't support it.

If any 3rd party has demo for it, welcome to share here.

 

0 件の賞賛
返信