MCUXpresso 11.3.0 mexfile is not being re-created

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MCUXpresso 11.3.0 mexfile is not being re-created

1,571件の閲覧回数
1234567890
Contributor IV

After exporting a project from 11.2.1 and importing in 11.3.0 I had some weird warnings:

1234567890_0-1611479427563.png

Tooltip: "Currently, there are 1 error and 0 warning".

1234567890_1-1611479500043.png

But Problems view ist empty.

So I deleted the mexfile as recommended here: https://community.nxp.com/t5/MCUXpresso-IDE/How-do-I-get-MCUXpresso-to-ignore-the-MEX-file/m-p/83540...

But then I get this error and have to restore the old mexfile.

1234567890_2-1611479618751.png

 

ラベル(1)
0 件の賞賛
返信
4 返答(返信)

1,569件の閲覧回数
1234567890
Contributor IV

Update (edit post no longer possible?):

The workspace-log says just before the error-message:

!MESSAGE The project 'xxx' does not contain any SDK reference or the SDK cannot be found.
!STACK 0

This error also occurs when clicking (project in Project Explorer highlighted):

1234567890_0-1611480405264.png

 

 

 

0 件の賞賛
返信

1,550件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi

From the error message, the problem could be related with SDK.

what's the SDK version do you used on MCUXpresso IDE 11.3.0 and 11.2.1?

What's the part number?

 

Thanks,

Jun Zhang

0 件の賞賛
返信

1,538件の閲覧回数
1234567890
Contributor IV

Hi,

sorry for incomplete information: On 11.3.0 I installed 2.9.0 and on 11.2.1 2.8.0 SDK LPC845BREAKOUT.

0 件の賞賛
返信

1,529件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Now you use MCIXpresso IDE 11.3.0  + SDK 2.9.0. Both of your IDE and SDK are updated.

With this new SDK, I suggest you create a new  project and import your own code into it. 

When you decide to start a new project with a specific version of SDK, we suggest you continue with it. sometimes a new version of SDK may change files or structure or function name, it potentially brings you trouble. If for some reason you must change SDK version, create a new project under new version of SDK then import your code part by part into it. This can save engineers workload from long term view.

 

Have a nice day,

Jun Zhang

 

0 件の賞賛
返信