MCULINK PRO DEBUG PROBLEM

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MCULINK PRO DEBUG PROBLEM

5,923 Views
emfact
Contributor II

I am using LPC5506 with SDK example,

I am able to flash it using Flash tool in MCUEXPRESSO and output is also ok.

But unable to DEBUG it. I am getting following error.

Target error from Commit Flash write: Ep(04). Cannot halt processor.

ERROR SCREENSHOT ATTACHED.

Please help me out.

Thank you

 

0 Kudos
Reply
6 Replies

5,889 Views
RaRo
NXP TechSupport
NXP TechSupport

Hello @emfact,

Could you please try the following suggestions? 1. Please double check that you stop previous debugging session instance before trying to run a new one. 2. Delete the .launch of the project and try to debug again. 3. Try out another example like a Hello World to see if the problem continues.

If the problem persists, could you please share your project?

Best regards, Raul.

0 Kudos
Reply

5,873 Views
emfact
Contributor II

 

Dear 

I had tried all 3 options you have mentioned but no luck.

Following GDB protocol problem is seen in console .

I am sharing console details 

 

Flash Write Done
Flash Program Summary: 22824 bytes in 0.06 seconds (348.27 KB/sec)
Starting execution using system reset and halt target with a stall address
Retask read watchpoint 1 at 0x50000040 to use for boot ROM stall
state - running or following reset request - re-read of state failed - rc Nn(05). Wire ACK Fault in DAP access
state - running or following reset request - re-read of state failed - rc Nn(05). Wire ACK Fault in DAP access
Warning - processor did not halt - gave up waiting
flash - system reset failed - Ep(04). Cannot halt processor.
Target error from Commit Flash write: Ep(04). Cannot halt processor.
GDB stub (C:\nxp\MCUXpressoIDE_11.6.1_8255\ide\plugins\com.nxp.mcuxpresso.tools.bin.win32_11.6.1.202210030617\binaries\crt_emu_cm_redlink) terminating - GDB protocol problem: Pipe has been closed by GDB.
state - running or following reset request - re-read of state failed - rc Nn(05). Wire ACK Fault in DAP access

 

0 Kudos
Reply

5,863 Views
RaRo
NXP TechSupport
NXP TechSupport

Hello @emfact,

Could you please tell us what board are you using? Is it a custom board or is it a NXP development board?

At the meantime, could you please try performing a mass erase to the flash memory using the GUI Flash Tool before debugging?

Finally, could you try updating the firmware of the MCU-Link Pro? For this, please refer to the following links: Getting Started with the MCU-Link Pro and MCU-Link Pro User Manual.

Best regards, Raul.

0 Kudos
Reply

5,844 Views
emfact
Contributor II

Dear RaulRomero

It worked after changing settings in debug configuration.

Attached my settings.

 

Thanks for your support

Regards

Hraj

Emfact

5,893 Views
Jadke09
Contributor I
I have some questions about the TJA1145T/FD, hope you can help. Should PNC and WUF be used together? If we want to use WUF https://testmyspeed.onl/ function, should we also use PNC?
0 Kudos
Reply

5,884 Views
RaRo
NXP TechSupport
NXP TechSupport

Hi @Jadke09 ,

Could you please create a new post in the following community: https://community.nxp.com/t5/Other-NXP-Products?

Regards, Raul.

0 Kudos
Reply