Dual-single-ended mode for LPC55s69's ADC

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Dual-single-ended mode for LPC55s69's ADC

1,096 Views
plong44
Contributor II

I am attempting to use the ADC in dual single ended mode (user manual section 39.6.16, ADC command low buffer registers, CTYPE == 0x03) on the LPC55s69 but so far I have not been successful. Other chips in the family (LPC553x) appear to have a very similar ADC and have a few added bits/fields in the same register that seem to pertain to this mode. But the corresponding bits/fields in the LPC55s69's user manual are reserved.

Has anyone else had any success using the ADC in dual single ended mode? Is this feature not supported in the LPC55s69?

0 Kudos
Reply
1 Reply

1,078 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @plong44 

You can try to use MCUXpresso config tool for peripheral to config:

Alice_Yang_0-1673334480070.png

 

BR

Alice

 

0 Kudos
Reply