MCULINK PRO DEBUG PROBLEM

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MCULINK PRO DEBUG PROBLEM

6,129件の閲覧回数
emfact
Contributor II

I am using LPC5506 with SDK example,

I am able to flash it using Flash tool in MCUEXPRESSO and output is also ok.

But unable to DEBUG it. I am getting following error.

Target error from Commit Flash write: Ep(04). Cannot halt processor.

ERROR SCREENSHOT ATTACHED.

Please help me out.

Thank you

 

0 件の賞賛
返信
6 返答(返信)

6,095件の閲覧回数
RaRo
NXP TechSupport
NXP TechSupport

Hello @emfact,

Could you please try the following suggestions? 1. Please double check that you stop previous debugging session instance before trying to run a new one. 2. Delete the .launch of the project and try to debug again. 3. Try out another example like a Hello World to see if the problem continues.

If the problem persists, could you please share your project?

Best regards, Raul.

0 件の賞賛
返信

6,079件の閲覧回数
emfact
Contributor II

 

Dear 

I had tried all 3 options you have mentioned but no luck.

Following GDB protocol problem is seen in console .

I am sharing console details 

 

Flash Write Done
Flash Program Summary: 22824 bytes in 0.06 seconds (348.27 KB/sec)
Starting execution using system reset and halt target with a stall address
Retask read watchpoint 1 at 0x50000040 to use for boot ROM stall
state - running or following reset request - re-read of state failed - rc Nn(05). Wire ACK Fault in DAP access
state - running or following reset request - re-read of state failed - rc Nn(05). Wire ACK Fault in DAP access
Warning - processor did not halt - gave up waiting
flash - system reset failed - Ep(04). Cannot halt processor.
Target error from Commit Flash write: Ep(04). Cannot halt processor.
GDB stub (C:\nxp\MCUXpressoIDE_11.6.1_8255\ide\plugins\com.nxp.mcuxpresso.tools.bin.win32_11.6.1.202210030617\binaries\crt_emu_cm_redlink) terminating - GDB protocol problem: Pipe has been closed by GDB.
state - running or following reset request - re-read of state failed - rc Nn(05). Wire ACK Fault in DAP access

 

0 件の賞賛
返信

6,069件の閲覧回数
RaRo
NXP TechSupport
NXP TechSupport

Hello @emfact,

Could you please tell us what board are you using? Is it a custom board or is it a NXP development board?

At the meantime, could you please try performing a mass erase to the flash memory using the GUI Flash Tool before debugging?

Finally, could you try updating the firmware of the MCU-Link Pro? For this, please refer to the following links: Getting Started with the MCU-Link Pro and MCU-Link Pro User Manual.

Best regards, Raul.

0 件の賞賛
返信

6,050件の閲覧回数
emfact
Contributor II

Dear RaulRomero

It worked after changing settings in debug configuration.

Attached my settings.

 

Thanks for your support

Regards

Hraj

Emfact

6,099件の閲覧回数
Jadke09
Contributor I
I have some questions about the TJA1145T/FD, hope you can help. Should PNC and WUF be used together? If we want to use WUF https://testmyspeed.onl/ function, should we also use PNC?
0 件の賞賛
返信

6,090件の閲覧回数
RaRo
NXP TechSupport
NXP TechSupport

Hi @Jadke09 ,

Could you please create a new post in the following community: https://community.nxp.com/t5/Other-NXP-Products?

Regards, Raul.

0 件の賞賛
返信