MCUExpreso Configure CTIMER

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MCUExpreso Configure CTIMER

3,940 次查看
PedroBecerra
Contributor III

I'm trying to configure a CTIMER as periodic timer in a LCP5516JBD100 processor.
I don't whant to move any output.

In the user manual I understand that it it possible, but MCUexpreso shows a warning: matchChannel: Match output of the match 0 channel of peripheral CTIMER0 is not routed.

Why?

How can I fix this?

Than you.

标签 (1)
0 项奖励
回复
2 回复数

3,908 次查看
PabloAvalos
NXP TechSupport
NXP TechSupport

Hi @PedroBecerra 

 

I would like to apologize for the delay. We are overloaded on the requests theses days. I really really appreciate your patience.

 

Regarding your questions, it is probably due to you did not turn on first the clock source for that peripheral, as you are using the config tool, on the peripheral side, you will need to enable the path for the clk on the clocks tab on config tools for that CTIMER0. Please try to enable it and tell me if you could solve it.

 

Please let me know if the problem still persist, so I can help you with.

 

Thank you.
Best Regards.
Pablo Avalos.

0 项奖励
回复

3,629 次查看
PedroBecerra
Contributor III

Hi Pablo.
That is not my problem.

The timer works fine, but I should give a gpio to move, and I don't want to move any gpio. I just want a timer irq.

Wy I get a warnig if I don't use a GPIO?

0 项奖励
回复