MAC/PHY Filtering

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MAC/PHY Filtering

1,352件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by jnewell on Fri Sep 20 11:20:26 MST 2013
Hey,

Has anyone experimented with filtering out packets from a specific ip addresses with the LPC1768 and LAN8720? (I'm using lwip and freeRTOS)

I'm having an issue when one of my high bandwidth streaming devices is running on the network at the same time that I'm trying to receive a different stream, seems like the PHY is just constantly receiving stuff, and the processor can't keep up with it.

If I use a multicast switch, I don't have the problem because then my device only receives packets from the specific multicast group that it joins.

-Josh
ラベル(1)
0 件の賞賛
返信
1 返信

1,267件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by MikeSimmonds on Sat Sep 21 04:52:09 MST 2013
You can't filter out, but you can filter in.

Set your boards MAC address in to the three station registers
[NB recall the reversing issue thread http://www.lpcware.com/content/forum/lan8720a-issues post 16]
and set to allow only unicast multicast and broadcast as shown in the same post.

You need broadcast for ARP requests so the remote sender(s) can get the MAC addr for the IP addr.

Then only packets addressed to your IP will be received and passed on to the CPU.

You'll have to dig into LWIP to see where this should be done [probably a LPC176X specific file to do with EMAC init]

Hope this will help.
0 件の賞賛
返信