Lpc4357 Can

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Lpc4357 Can

Jump to solution
3,421 Views
Newton829
Contributor II

Hello All,

   In the user manual of LPC4357,under CAN section .

There is a CAN_CLK register, which specifies the devision of Peripheral clock.

Similar under CAN_BT ther3 are bits for baud rate prescaler.

 

Can some one please explain me are these register same? As the seems to do the same job or do they serve any different purpose

2.For the calculation of Timming parameters of Can do I need to the total of both the devisor?

Thank you

 

Labels (4)
Tags (1)
0 Kudos
Reply
1 Solution
3,413 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

For the CAN bus driving clock of LPC43xx, I suppose that this is the CAN clock divider map for CAN0 module:

                                   Divider1                                                     Divider2

BASE_APB3_CLK---[DIVVAL bits in CAN_CLK register]---[BRP bits in C_CAN0_BT register]--Tq clock

For the Divider1:

xiangjun_rong_1-1669788072266.pngxiangjun_rong_1-1669788072266.png

 

 

For the Divider2

xiangjun_rong_0-1669787948905.pngxiangjun_rong_0-1669787948905.png

 

For the BASE_APB3_CLK source selection, pls refer to

xiangjun_rong_2-1669788394599.pngxiangjun_rong_2-1669788394599.png

 

Hope it can help you

BR

XiangJun Rong

View solution in original post

0 Kudos
Reply
1 Reply
3,414 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

For the CAN bus driving clock of LPC43xx, I suppose that this is the CAN clock divider map for CAN0 module:

                                   Divider1                                                     Divider2

BASE_APB3_CLK---[DIVVAL bits in CAN_CLK register]---[BRP bits in C_CAN0_BT register]--Tq clock

For the Divider1:

xiangjun_rong_1-1669788072266.pngxiangjun_rong_1-1669788072266.png

 

 

For the Divider2

xiangjun_rong_0-1669787948905.pngxiangjun_rong_0-1669787948905.png

 

For the BASE_APB3_CLK source selection, pls refer to

xiangjun_rong_2-1669788394599.pngxiangjun_rong_2-1669788394599.png

 

Hope it can help you

BR

XiangJun Rong

0 Kudos
Reply