Lpc 824 DMA to GPIO

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Lpc 824 DMA to GPIO

5,069件の閲覧回数
tvrklejelani
Contributor I

Hi,

i have problems driving lpc gpio port using dma. When i write with dma to any ram adress everything  works fine, but when i write to any of registers associated with gpio nothing happens.

My question is... Can 824 use dma to write to gpio.

Based on block diagram of 824, GPIO is connected to ARM M0+ but not to AHB..is this true?

Thx.

ラベル(1)
4 返答(返信)

4,756件の閲覧回数
tvrklejelani
Contributor I

Hi, it was a couple of years now, but for 824 it can't use DMA to access gpio, i was always getting dma erros.

And reason is that GPIO is "tightly" coupled to core. 

If your LPC has same architecture as on picture above, than i think it can not work. 

But if GPIO is connected to AHB bus and DMA is connected to it it might work. 

Does that uC has DMA?

BR/Tvrtko

4,756件の閲覧回数
javiervallori
Contributor III

Thank you! the uC has a DMA, and the GPIO seems to be connect to the AHB. But for some reason, setting DMA destination address to the GPIO has no effect.

0 件の賞賛
返信

4,756件の閲覧回数
javiervallori
Contributor III

Did you finally find a solution? I'm having the same problem with a LPC11

0 件の賞賛
返信

4,756件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi Tvrkle JElani ,

Thank you for your interest in NXP Semiconductor products and the opportunity to serve you.

In my opinion, the GPIO is connected to the APB bus, and it can work with the DMA engine.

Hope it helps.
Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信