Low Pin count uC with LF Osc?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Low Pin count uC with LF Osc?

1,400 Views
richardsoennich
Contributor I

Does the LPC line include a model with low pin counts and a LF osc (with XTAL pins, for 32.768 KHz xtal)?

I need a real RTC....

Thanks

Rich

0 Kudos
Reply
1 Reply

1,324 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Richard,

First of all, we have the dedicated RealTimer/Calendar chip PCA family with IIC or SPI interface, pls refer to the link:

Automotive RTCs | NXP 

Secondly, as you know that the LPC family is a Micro Controller family, but some of them have the on-chip RealTimer/Calendar module. The LPC8N04 is a low pins low cost processor with on-chip RTC powered by battery pin.

Pls refer to the link:

LPC8N04 8 MHz |Arm® Cortex®-M0+|32-bit Microcontrollers (MCUs) | NXP 

Hope it can help you

BR

Xiangjun Rong

0 Kudos
Reply