Linux cmd tool to flash LPC546xx

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Linux cmd tool to flash LPC546xx

1,250 Views
arthuraner
Contributor I

In the manual it's said that ISP is possible wiht USB, is there a linux commandline tool or so where I can give my .axf file as an argument and program the flash? It's a LPC546xx 

0 Kudos
Reply
1 Reply

1,134 Views
brendonslade
NXP TechSupport
NXP TechSupport

Is mass storage boot a viable way for you to work? Then the device will just appear like a mass storage drive; you delete the firmware.bin file you will see there, then replace it with your application, renamed to firmware.bin.

Not sure why you have to have .axf files ... MCUXpresso IDE will generate a bin file for you automatically - right click on the axf file and select Binary Utilities > Create binary to get it.

0 Kudos
Reply