Linux cmd tool to flash LPC546xx

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Linux cmd tool to flash LPC546xx

1,249件の閲覧回数
arthuraner
Contributor I

In the manual it's said that ISP is possible wiht USB, is there a linux commandline tool or so where I can give my .axf file as an argument and program the flash? It's a LPC546xx 

0 件の賞賛
返信
1 返信

1,133件の閲覧回数
brendonslade
NXP TechSupport
NXP TechSupport

Is mass storage boot a viable way for you to work? Then the device will just appear like a mass storage drive; you delete the firmware.bin file you will see there, then replace it with your application, renamed to firmware.bin.

Not sure why you have to have .axf files ... MCUXpresso IDE will generate a bin file for you automatically - right click on the axf file and select Binary Utilities > Create binary to get it.

0 件の賞賛
返信