Letter of Volatility-LPC178x/7x

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Letter of Volatility-LPC178x/7x

2,556 Views
brad_sweigert
Contributor I

Hello,

I'm trying to obtain what's called a letter of volatility (LoV) for the referenced controller.  This letter or statement would break down the various memory modules that are present as well as details as to whether or not the memory space is accessible, whether it's volatile or non-volatile, and any methods required to clear or sanitize said memory space.  I can go through the manual and see the various types of memory that are present and the function the memory serves but was looking for a standalone document of some sort that specifically relates and provides details into the memory components.

Thanks in advance!

Labels (1)
0 Kudos
Reply
2 Replies

2,491 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Brad,

Unfortunately, I have not found any letter of volatility, but in the data sheet of LPC17xx, there is memory map section, which define the memory location for on-chip ROM, flash, SRAM and external memory space for SDRAM or SRAM.

For example, this is the memory map screenshot in data sheet.

Hope it can help you

BR

XiangJun Rong

pastedImage_1.png

0 Kudos
Reply

2,491 Views
brad_sweigert
Contributor I

Thank you for the quick reply!  I think this is about as close as I'll get to an LoV.  Appreciate the help!

0 Kudos
Reply