LWIP Example for LPC11U68?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LWIP Example for LPC11U68?

2,698件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by danielmo on Tue May 31 07:10:55 MST 2016
Hi everyone,

i am using LPCXpresso v 8.1.4 and i wonder if there is an example project with LWIP for the LCP11U68 microcontroller. The archive "Examples/LPCOpen/lpcopen_2_06_lpcxpresso_manley_11u68.zip" and ""Examples/LPCOpen/lpcopen_2_06_lpcxpresso_nxp_lpcxpresso_11u68.zip" does not seem to contain an lwip-example project. However, the archive for the 1769  located in "Examples/LPCOpen/lpcopen_2_10_lpcxpresso_nxp_lpcxpresso_1769.zip" has one.

Is it usable for the 11u68 too?

regarts
Daniel
ラベル(1)
0 件の賞賛
返信
4 返答(返信)

2,602件の閲覧回数
lpcware
NXP Employee
NXP Employee
bump
0 件の賞賛
返信

2,602件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by R2D2 on Wed Jun 01 16:11:06 MST 2016

Quote: danielmo
Does it mean, the 1769 has already a build in MAC interface...



Yes...


Quote: danielmo
If it is so, would it be nesseccarry to equip the 11u68 with an external module, maybe an ENC28j60, and write a driver for it and a driver for the 11u68 in order to get it working with lwip?



ENC28J60 has a SPI interface, Google will probably help you to find samples  :)
0 件の賞賛
返信

2,602件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by danielmo on Tue May 31 08:23:34 MST 2016
Well okay. Does it mean, the 1769 has already a build in MAC interface (or at least anything that is capable of doing networking) and the 11u68 not? If it is so, would it be nesseccarry to equip the 11u68 with an external module, maybe an ENC28j60, and write a driver for it and a driver for the 11u68 in order to get it working with lwip?
0 件の賞賛
返信

2,602件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by R2D2 on Tue May 31 07:32:35 MST 2016

Quote: danielmo
Is it usable for the 11u68 too?



:D

LPC11U68 has no 'Ethernet block'...
0 件の賞賛
返信