LWIP Example for LPC11U68?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LWIP Example for LPC11U68?

2,794 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by danielmo on Tue May 31 07:10:55 MST 2016
Hi everyone,

i am using LPCXpresso v 8.1.4 and i wonder if there is an example project with LWIP for the LCP11U68 microcontroller. The archive "Examples/LPCOpen/lpcopen_2_06_lpcxpresso_manley_11u68.zip" and ""Examples/LPCOpen/lpcopen_2_06_lpcxpresso_nxp_lpcxpresso_11u68.zip" does not seem to contain an lwip-example project. However, the archive for the 1769  located in "Examples/LPCOpen/lpcopen_2_10_lpcxpresso_nxp_lpcxpresso_1769.zip" has one.

Is it usable for the 11u68 too?

regarts
Daniel
Labels (1)
0 Kudos
Reply
4 Replies

2,698 Views
lpcware
NXP Employee
NXP Employee
bump
0 Kudos
Reply

2,698 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by R2D2 on Wed Jun 01 16:11:06 MST 2016

Quote: danielmo
Does it mean, the 1769 has already a build in MAC interface...



Yes...


Quote: danielmo
If it is so, would it be nesseccarry to equip the 11u68 with an external module, maybe an ENC28j60, and write a driver for it and a driver for the 11u68 in order to get it working with lwip?



ENC28J60 has a SPI interface, Google will probably help you to find samples  :)
0 Kudos
Reply

2,698 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by danielmo on Tue May 31 08:23:34 MST 2016
Well okay. Does it mean, the 1769 has already a build in MAC interface (or at least anything that is capable of doing networking) and the 11u68 not? If it is so, would it be nesseccarry to equip the 11u68 with an external module, maybe an ENC28j60, and write a driver for it and a driver for the 11u68 in order to get it working with lwip?
0 Kudos
Reply

2,698 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by R2D2 on Tue May 31 07:32:35 MST 2016

Quote: danielmo
Is it usable for the 11u68 too?



:D

LPC11U68 has no 'Ethernet block'...
0 Kudos
Reply