LQFP208 Package Question

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LQFP208 Package Question

1,825件の閲覧回数
754544799
Contributor I

LQFP208 Package.jpg

Hi,I want to confirm is the LQFP208 Package drewing topview or bottomview in the “SOT459-1.pdf”.

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,754件の閲覧回数
soledad
NXP Employee
NXP Employee

Hi,

the LQFP208 Package drewing is topview


Have a great day,
Sol

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信

1,754件の閲覧回数
maxintelcpu
Contributor I

Hi,

I want to get the ".step" file of the package.

Thank you!

0 件の賞賛
返信