LPCxpresso54628 program

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPCxpresso54628 program

1,431 Views
padmaashok765
Contributor II

Hi,

I am using LPCxpresso54628 development board. I have tested the example programs and are working fine.

I face difficulty to write my own program in accessing registers. I don't know how to access each bit of a register. I am using LPC54628.h header file which i got with xpresso sdk package. I need an led toggle program. Suggest me if some other header files is available.

Can any one help me with this.

Thanks in advance.

Labels (2)
0 Kudos
Reply
1 Reply

1,338 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello padma priya ,

Please refer to the gpio_led_output demo under SDK.

There is gpio drivers you can use to control GPIO( for example GPIO_PortSet(), GPIO_PortClear(),GPIO_PortToggle() and so on. )

If you want to directly config registers, you can refer to the drivers, for example, config the " GPIO port toggle registers":

pastedImage_3.png

Hope it helps,

Have a great day,
TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply